QTM Quick Connect Press Temp Rating
Change to QTM Series Quick-Connects Pressure and Temperature Rating
Notification of Change
We are pleased to inform you that the temperature rating of the PTFE sealed QTM series quick connect will increase from a maximum of 120°F (48°C) to a maximum of 350°F (176°C) at a pressure rating of 800 psig (55.1 bar). All other ratings will remain the same. Refer to the chart below or product catalog for details.
This change is a result of expanded validation testing of the current design. No design changes were made to the product in order to achieve this extended temperature rating.
Product literature, MS-01-138, has been updated. There are no changes on how you order these items.