GB Series Ball Valve
Product Update: Gaugeable Preswage Tool
This tool has an updated design
The gaugeable preswage tool is moving from a one-piece body design to a two-piece design except for the sizes noted in the table below, similar to the design used in the standard preswage tool. The new design uses a machined insert that is pressed into a cast body. This will result in an improvement in manufacturing output.
All functional dimensions are remaining the same. However, there will be a visual and physical difference for the tool as shown in the picture below (greater overall length and body diameter). There is no impact to product function. Ordering numbers will remain the same.
New 1/2" Gaugeable Preswage Tool
Old 1/2" Gaugeable Preswage Tool